Trends UI
The Trends user interface consists of a trends display pane and a Trend Library pane.
Trends display pane
The Trends display pane shows the trends selected in the Trend Library. When you create a trend, it automatically opens in the display pane and the trend name is selected in the Trend Library. You can select multiple trends to be shown simultaneously in the display pane. Scroll the display pane to view all of the trends that you selected in the Trend Library. For information on the options and controls available in the trend view, see Trends options.
If you log out of the application, your selections are retained and are loaded in the Trends display pane the next time you log in.
Trend Library
The Trend Library contains all the trends that are configured in the system. Trends can be listed individually or they can be organized within folders. You use the Trend Library to select the trends you want to view.
TIP: To hide the library, click the Hide Library icon (
or
) in the top right corner of the library. To show the library, click the Show Library icon (
or
) at the top of the library ribbon, or click anywhere in the minimized library ribbon.
For information on how to configure Trends, see Trends configuration.